5/2/2019 6:48 AM | |
Posts: 21 Rating: (0) |
Hi All , I am using TP1200 Comfort panel, i want to download my backup from usb. 1. i created a pack and go zip file of the backup 2. Move the file in the usb and insert the usb into HMI 3. Change the trasfer settings to USB device in control panel of HMI 4. Open Service and Commissioning / load project from external Device / select usb / scanning. 5. After i select USB and go next , it start scanning and keep on scanning i waited around 40 min. 6. Am i following the correct procedure. i already checked the link :https://support.industry.siemens.com/cs/ww/en/view/58876345 Please let me know if there is any other way. Thanks |
Last edited by: Prattsega at: 05/02/2019 06:53:56Last edited by: Jen_Moderator at: 05/02/2019 12:31:15Optimized link. |
|
5/2/2019 8:36 AM | |
Joined: 4/24/2006 Last visit: 9/13/2024 Posts: 8736 Rating: (1167) |
Hello, Did you make a Pack and Go file? Or did you perform a Backup from panel to USB stick? Best regards, Wizard |
5/3/2019 6:59 AM | |
Posts: 21 Rating: (0) |
Hello Wizard, I created pack and go file. |
5/3/2019 7:07 AM | |
Joined: 9/22/2014 Last visit: 6/12/2024 Posts: 89 Rating: (13) |
Dear Prattsega, For the Comfort panel and if you are using V14 or above then go through the following link to download the program in your comfort panel using memory device. https://support.industry.siemens.com/cs/cn/en/view/109740696 Hope this will help you. Thanks. |
Last edited by: Jen_Moderator at: 05/03/2019 10:12:17Optimized link. |
|
This contribution was helpful to2 thankful Users |
5/3/2019 7:28 AM | |
Posts: 21 Rating: (0) |
Hello . Thanks , It worked. |
Follow us on