6/3/2019 12:00 PM | |
Posts: 3 Rating: (0) |
Hi, i need to communicate my PLC 314C-2PN/DP with HMI and PC via Modbus. Should i need Modbus licence or Modbus Network Card? Thanks. |
6/3/2019 1:13 PM | |
Joined: 4/24/2006 Last visit: 5/1/2024 Posts: 8629 Rating: (1147) |
Hello, Have you seen this link: https://support.industry.siemens.com/cs/nl/nl/view/22660304/en Best regards, Wizard |
6/5/2019 10:33 AM | |
Posts: 3 Rating: (0) |
Thank you very much, Best regards. |
6/5/2019 10:40 AM | |
Posts: 3 Rating: (0) |
Hi, I have already seen the link but that is about other brand dispositive connection. What i was referring to is the connection of Siemens 314C-2 PN/DP to PC or Siemens HMI via Modbus. Thanks. |
Last edited by: anderpy at: 06/05/2019 10:40:32 |
|
6/5/2019 12:40 PM | |
Joined: 4/24/2006 Last visit: 5/1/2024 Posts: 8629 Rating: (1147) |
Hello, Here is a manual: SIMATIC HMI WinCC flexible 2008 Communication Part 2 See chapter 6 for communication Modbus. Why would you want to use Modbus communication, when you have Siemens PLC and HMI? Best regards, Wizard |
6/5/2019 12:49 PM | |
Posts: 3093 Rating: (322)
|
Block library for Modbus/TCP communication via the integrated PN interface of a SIMATIC CPU |
Follow us on