(0)| 10/16/2008 12:43 PM | |
|
Joined: 9/27/2006 Last visit: 1/14/2026 Posts: 12480 Rating:
|
hello Yai; You can configure "Universal Module" if you do not find the correct module in the HWConfig; just make sure you setup the correct number of bytes (I and Q) required to operate this module. The IM 308C configuration is done with Com Profibus, and downloaded to the module's memory card. Here is a sample program from Siemens showing how to set theIM 308C as a slave to a 315-2DP; it also discusses the use of Universal Modules in the S7 master configuration: http://support.automation.siemens.com/WW/view/en/6556876 Hope this helps, Daniel Chartier |
Follow us on