7/2/2019 9:51 AM | |
Joined: 2/18/2015 Last visit: 12/6/2023 Posts: 11 Rating: (2) |
Hello Guys. I trying build S7 communication between RTX V4.6 and S7-1200 CPU for data exchange. Everything is looking good but : -RTX is active ends station - connection is not established and I can't check why. - is it possible to use IE general as submodule ( Win AC version 4.6, SIMATIC NET V7.1.6 HF1 )? IE General is not available in WinLC properties ( check screenshot ). - on connection diagnostic in TIA V13 I see status only one connection ( CPU1200 --> RTX ), second one status is not available. Why ? ( check attachment ) Could you help me ?? Thx. Attachmentscreenshots.zip (949 Downloads) |
Follow us on