6/27/2019 12:35 PM | |
Joined: 3/3/2017 Last visit: 2/28/2024 Posts: 18 Rating: (0) |
I am commissioning 840dsl V4.8, upon having old backup of 840Dpl i want to know the NC variable which are transferred to DB120,in FB2. .I am attaching a pdf of DB120,I want to know that to which nc variable this refers(which nc variable is accessed in DB120). I am having NC-Var selector tool along if I can find through it pls share the procedure. AttachmentDB120.pdf (122 Downloads) |
Last edited by: Jen_Moderator at: 07/02/2019 14:03:55Optimized headline. |
|
6/27/2019 2:26 PM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (873)
|
Could you please attach your old 840D PL project back up here? |
7/1/2019 6:48 AM | |
Joined: 10/27/2009 Last visit: 3/15/2024 Posts: 455 Rating: (77) |
The attached DB120 contains five variables "measPos1" (Encoder position of Enc 1) for axes 1..5 |
hope that helps |
|
7/6/2019 10:11 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (873)
|
HelloCNC600, Thanks for the reply. Please could you expalin it little bit more like, how bereich_u_einheit : BYTE := B#16#1; is derived as // Area: N? how spalte : WORD := W#16#5; derived as // VariableName measPos1? how bausteintyp : BYTE := B#16#71; is derived as // Component SEMA? Thanks in advance. |
Follow us on