8/7/2019 6:40 AM | |
Joined: 8/1/2012 Last visit: 4/18/2024 Posts: 76 Rating: (3) |
For multimode olm, either om2 or om3 or om4 will work right? Regards, wantutri ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 08/07/2019 07:13:34New subject after splitting |
|
8/8/2019 8:14 AM | |
Joined: 8/3/2009 Last visit: 5/24/2024 Posts: 12981 Rating: (1653) |
Hello wantutri The Topic you are referring is almost 10 years old. What do you mean with "will work right....."?? Whats your usecase, which Devices do you use? Can you please describe your question with more details...? Thanx Murof |
If this Information really helps, you could use the Rate function |
|
8/8/2019 12:53 PM | |
Joined: 9/27/2006 Last visit: 5/26/2024 Posts: 12257 Rating: (2668) |
Hello wanturi; Compare the tables from the Siemens OLM manual (as attachment below) and form the Cablek corporation (makers of F,O, cable), in the following links: https://support.industry.siemens.com/cs/us/en/view/109476821 http://www.cablek.com/technical-reference/fiber-/fiber-optic-cable-types Basically, multimode cable with core 50-125um (OM2) or 65-125um (OM1) can be used with the G11, G12 and G22 OLM transmitters. Hope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
Follow us on