9/7/2019 10:17 AM | |
Joined: 8/25/2019 Last visit: 1/22/2024 Posts: 4 Rating:
|
Dear Sir I am using Matsterdrive mc compact plus and Chasis units for sheet cutter application, we parameterized with 368=3 ,On command via DI-X101-8-P554=20speed set point via MOPX101- DI6-P573=14 &X101- DI7-P574=16 for speed raise and lower and main set point connector KK0058 Aalso put in P443, first time drive was started and speed also increased/decreased,we restarted the drive second time drive is ON but speed is not increased and decreased but inputs are coming and checked with r550 is ok and speed set point is not coming at r424 when push the buttons of raise and lower,please and PMU is flashing 1 and -0 continuously give me solution to run the system Thanks & Regards S.Thangamani
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/09/2019 11:33:36New subject after splitting |
|
9/7/2019 11:23 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating:
|
Hello Gold Bell, Please do not create multiple posts & never create in old topic. Instead always use to post your query in new topic. Now to your query - MOP DI terminal 6 is DI 4 & its BI = 16 not 14. Also DI terminal 7 is DI 5 & its BI = 18 & not 16. So p573 must be 16 & p574 must be 18. Please check & confirm. |
Follow us on