8/23/2012 10:54 AM | |
Joined: 7/9/2012 Last visit: 5/10/2019 Posts: 12 Rating: (0) |
I've got the answer to my question. In attachement the solution (in dutch :s) In fact i want to do the same homing (by using thehmi)like you can do with the control panel. The solution is to use the block _Homing. Regards AttachmentC:\Users\kdb.DELTA\Desktop\Absolute encoder offset.pdf (656 Downloads) |
Follow us on