9/12/2019 11:44 AM | |
Joined: 1/23/2009 Last visit: 6/3/2024 Posts: 6 Rating: (0) |
Hello, I have the same problem with S1518F and 2 scalances. The message "wrong partner" is sporadic. It can have a duration of 20 seconds , 1 time per day. Topology is configured and correct. Scalance is configured as Device IO. The problem happened when I configured it as an IO device. I configured it like this to avoid having the defect led on the scalance What can I do ? Damien ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/12/2019 13:42:07New subject after splitting |
|
Follow us on