9/19/2019 2:18 PM | |
Posts: 2 Rating: (0) |
The Siemens Simatic Field PG M6 Programming Device is offered in totally protected magnesium lodging with silver lodging spread and M6 engraving. The gadget accompanies fast DDR4 work memory of up to 32 GB and an effect safe SSD mass stockpiling up to 2 TB. The item is built for portable use in machines and plants for arrangement, charging, administration and upkeep. The Comfort form of the programming gadget highlights propelled interfaces, for example, RS 232, Profibus, Profinet, Simatic Card and WLAN 802.11ac remote and BT V5.0 Bluetooth innovation. ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 09/20/2019 16:35:32New subject after splitting |
|
Follow us on