11/17/2008 11:33 AM | |
Posts: 14 Rating:
|
Hello Daniel, I think you didnt understand me... I already make program for PLC (with Step7, using modbus libary), and download it to PLC (using RS232/PPI Multimaster Cable).... Now I want to see if the protocol is working.... so I will try to connect PLC with PC. My question is now: can I use the cable which I used for download program to PLC for modbus connecting PLC and PC . See atachment Attachmentcomunication.pdf (362 Downloads) |
11/18/2008 7:58 AM | |
Posts: 14 Rating:
|
Dear J_Bell thank you for yor help, i will see what will i do.... one more time, thanks |
Follow us on