1/4/2020 4:19 PM | |
Joined: 9/29/2011 Last visit: 1/23/2025 Posts: 6 Rating:
|
Hi folks, yesterday I made a simple test program to collect data from a serial device with my IOT2020. While my program was running fine with PL210x- and ftdi- USB-serial adapters plugged into the IOT, it failed with wrong received data on two CH34x-based adapters. Practically the same program under WINDOWS was working OK with all four adapters. Searching for the cause I found that in older LINUX distros a broken CH340 driver was included. Could you please check and update the driver and your distributed, precompiled images? And probably release a ch34x.ko to update the existing installations? I did not test that myself yet, as I first need to set up the full LINUX cross compilation environment to be able to compile the driver myself ... sorry, lack of time in the moment ... As more and more devices in the ARDUINO sphere and beyond are using these CH34x chips, users will appreciate it ...
tnx es 73, df5zx [tnx es 73 means thanks and best regards by radio amateur code , for those, who do no know :-) ] |
Last edited by: df5zx at: 01/04/2020 16:34:21 |
|
1/8/2020 10:11 AM | |
Joined: 12/12/2016 Last visit: 7/25/2025 Posts: 640 Rating:
|
Hello, Thanks for the hint. Could you please open an issue on here. Kind regards! |
This contribution was helpful to
1 thankful Users |
1/8/2020 10:28 PM | |
Joined: 9/29/2011 Last visit: 1/23/2025 Posts: 6 Rating:
|
Done ! |
Follow us on