2/12/2020 4:20 PM | |
Joined: 1/4/2013 Last visit: 9/9/2024 Posts: 1124 Rating:
|
Dear all, one of our customers, with a D410-2 and a KTP Comfort Panel, called us and said that the machine was stopped (HMI was not communicating). They powered off the machine and powered on again and everything was fine (the retentive variables were kept perfectly and machine was able to run). They asked me to analyze what happened and I found this line in the "Syslog" of the webserver of Simotion. check serial number: initialize nv-ram caused by detecting differences between serialclnumber of device and of file What it can be ? Is it the cause that made that condition ? In the attached file there is the syslog of all events Danke in advance Attachmentsyslog.txt (131 Downloads) |
Searching for Siemens used/new equipments ? |
|
Follow us on