2/15/2011 9:46 AM | |
Posts: 89 Rating: (4) |
How to extract the Hour , Minute , Date etc. Attached File is the Test Source File in which I was working Splitted from reading date and time in SCL. AttachmentTest.zip (1525 Downloads) |
Last edited by: O_Moderator at: 2/16/2011 9:20 AMnew subject after splitting |
|
2/15/2011 12:58 PM | |
Posts: 316 Rating: (37) |
I think the FCs "DT_DATE"(FC6), "DT_DAY"(FC7) and "DT_TOD"(FC8) can help you. This functions you can find in "Standard Library"--> "IEC Function blocks". If you need more inforamtion to this functions press the button "F1" while the function is marked. Also check this link: http://support.automation.siemens.com/WW/view/en/36479 --> Structure of Date_and_Time data type. |
Last edited by: Chilly_Garfield at: 2/15/2011 1:02 PM |
|
3/2/2011 9:42 AM | |
Posts: 3 Rating: (0) |
Thanks..FC6 helps to extract Date from Date and time format |
Follow us on