5/4/2020 8:19 PM | |
Posts: 24 Rating: (0) |
Hello All, I have CPU 1200, and I want to change the IP address of the PLC and HMI from 192.168.0.1 , .02 to 192.168.1.197 ,.198. I did change the IP addresses of the PLC and HMI in such a way that they are connected together.BUT, since it needs to stop PLC, after downloading the new hardware change, I COULD NOT change the PLC mode from stop to run mode. I tried, power off and on, downloading full software, memory reset, but by either way, I could not change the mode to run mode, and I had to bring back the IP address to old one and download again to be able to change the mode to run mode. Does anyone have a similar experience? Thanks in advance for any advice. Esi ------------------------------------------------------------------------------------------ |
Last edited by: EsiGh at: 05/04/2020 20:19:46Last edited by: EsiGh at: 05/04/2020 20:24:19Last edited by: Jen_Moderator at: 05/05/2020 09:55:39New subject after splitting |
|
5/5/2020 9:56 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
Closed cause question posted twice. The second thread with the subject Cannot place PLC to run mode is published within the conference SIMATIC S7-1200. Best regards,Jen_Moderator |
Follow us on