5/20/2020 6:46 PM | |
Joined: 1/10/2020 Last visit: 7/24/2024 Posts: 25 Rating: (0) |
hi, I'm new to using HSC, could you help me in the HW configuration of this encoder motor? https://content.ugfischer.com/cbfiles/fischer/Zulassungen/ft/153422-Encodermotor9V.pdf maybe I understood that I have to set up single phase, but it is not clear to me how to manage the DIR? thanks for any indication and suggestion? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/22/2020 07:28:08New subject after splitting |
|
5/21/2020 1:33 AM | |
Joined: 3/16/2015 Last visit: 10/10/2021 Posts: 1250 Rating: (173) |
Which PLC, Module or Board? Pay particular attention to voltage/resistor requirements detailed in the datasheet. Your encoder can only be setup for single phase and in that case there's no way to determine direction. |
This contribution was helpful to1 thankful Users |
5/21/2020 9:15 AM | |
Joined: 3/30/2020 Last visit: 9/26/2024 Posts: 4796 Rating: (984) |
Adding my opinion.. That motor is a 9V motor. The encoder is meant for 9V. The encoder signal is NPN. The description is less clear about using a 5V supply, where it is converted to PNP with a pull-up. I assume you can power the encoder with 5V. The resolution of the encoder is very bad. Using this motor is not a great idea. Does the project insists on it? You will need a signal board that handles the 5V signal of the encoder. You can leave the NPN signal as is. It is doubtful if you will need a HSC. If your project insists on using the base PLC only - you will need to build an electronic circuit to boost/amplify the encoder signal to 24V. Above 15V is TRUE and below 5V is FALSE. An opamp or transistor amplifier should work. The other consideration (best solution) would be to get an external encoder. You can make one yourself if needed. Mount the encoder on the outgoing shaft of the motor or whatever you need to move. Get all of the circuits in place first. Then test with the PLC that you get out some signal correctly. Only after can you concentrate on the coding. Good luck. |
Last edited by: qwazee at: 05/21/2020 09:18:53Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
This contribution was helpful to1 thankful Users |
5/21/2020 9:36 AM | |
Joined: 3/16/2015 Last visit: 10/10/2021 Posts: 1250 Rating: (173) |
It looks like a hobby project. |
5/21/2020 9:45 AM | |
Joined: 3/30/2020 Last visit: 9/26/2024 Posts: 4796 Rating: (984) |
If I showed you some of my projects, Highly possible it is a school project.
|
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
This contribution was helpful to1 thankful Users |
Follow us on