7/2/2012 8:30 PM | |
Joined: 6/4/2008 Last visit: 8/16/2024 Posts: 1492 Rating: (323)
|
Hi Andy, generally, upgrades to a higher firmware version are best done using the Drivemonitor convert function and usually don't have any issues. As you don't have v1.4, I have attached the file (Which is an executable, so please do scan it) With this, you can flash v1.4 firmware to the drive, and then try the backup download again. Sometimes, the earlier version of firmware cannot overwrite a later version (i.e. v1.4 on top of v1.6) Regards, Graeme
AttachmentMCP_V142.zip (715 Downloads) |
6/20/2016 1:58 PM | |
Posts: 1 Rating: (0) |
Does anybody knows there to find Masterdrives firmware version V1.5 ? |
6/21/2016 9:17 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (876) |
Hello, Direct link to MC v1.5 is not available. But please check below FAQ, it may help you. Release for the SIMOVIS start-up tool, Version V5.4 |
6/18/2020 6:50 AM | |
Joined: 10/29/2014 Last visit: 9/8/2022 Posts: 3 Rating: (0) |
Hello, Do you need the V1.53? |
Follow us on