12/15/2008 2:43 PM | |
Posts: 31 Rating: (0) |
Hi everybody, AttachmentSim_doc.zip (562 Downloads) |
12/18/2008 10:38 AM | |
Posts: 10 Rating: (0) |
Yes it's normal. With came there is 3 step : - Following axis is synchronizing on master - Following axis is synchronized - Following axis is unsynchronizing. In your program, if you enter 0 in synclengh, it mean that your slave has to reach instantaneouslythe master. So enter a little value, for ex. 50mm. You have to change the mode of caming too : Begin des Aufsynchronisierens : sofort. enclosed is a xmltest program. Attachmenttest.zip (450 Downloads) |
12/19/2008 11:30 PM | |
Posts: 31 Rating: (0) |
And could you please tell me how to export in in exel? |
1/7/2009 4:55 PM | |
Posts: 10 Rating: (0) |
hi, it's realy easy : right clic on your measure > export |
Follow us on