8/13/2020 8:31 AM | |
Posts: 1 Rating: (0) |
Hi, I'm having the similar issues on KTP700 as well. The alarm just won't go off on the panel. I create a panel of the alarm for the Pending Alarm and Unacknowledged Alarm for display and another is Buffer Alarm for the display. The buffer alarm have all acknowledged and cleared for the alarm but the panel for the alarm for the pending alarm and unacknowledged alarm still having one of the alarm staying there. I check thru the TIA Portal, the fault alarm logic have cleared the alarm in ladder as well. Tried to press the acknowledge button on the buffer alarm panel, still not removing the alarm on the alarm panel thou. Any solution on this? I searching on the forum, yet only found this thread and still without solution. ------------------------------------------------------------------------------------------ AttachmentAlarmNotGoingOff.zip (82 Downloads) |
Last edited by: Jen_Moderator at: 08/13/2020 09:00:34New subject after splitting Last edited by: K1230912019823 at: 08/14/2020 03:32:18- 14/8/2020 Update attachment with more images |
|
Follow us on