8/9/2020 2:29 PM | |
Posts: 10 Rating: (0) |
Hello Everybody. For last few days im trying to establish modbus connection Logo! and EasyIO FG32+ with no success. Probobly most of you guys don't come across with EasyIO controllers but at lest maybe someone help me with correct configuration of Logo. They both looks connected and see each other but no luck with read or write data, i try to use network input/output directly and also to read to VM of logo and from VM on diagram. Pictures and EasyIO pdf manuals in Zip. Thanks. AttachmentEasyIO Logo1.zip (153 Downloads) |
Last edited by: zigzak at: 08/09/2020 14:34:18 |
|
8/9/2020 2:31 PM | |
Posts: 10 Rating: (0) |
EasyIO manual.
Attachment03 EasyIO FG Series User Reference v1.7 (1).pdf (162 Downloads) |
8/9/2020 2:33 PM | |
Posts: 10 Rating: (0) |
EasyIO Modbus Master.
Attachment10 EasyIO FG Series Modbus Master v1.2 (4).pdf (166 Downloads) |
8/9/2020 2:33 PM | |
Posts: 10 Rating: (0) |
EasyIO slave.
Attachment11 EasyIO FG Series Modbus Slave v1.1 (1).pdf (154 Downloads) |
8/9/2020 5:27 PM | |
Joined: 2/22/2008 Last visit: 5/6/2024 Posts: 2698 Rating: (206) |
The EasyIO FG32+ seems to be an interesting device, but your uploaded instructions are sparely. I have seen, that the drivers for Modbus TCP must be installed on the device. On your hardcopies i cannot see, if this is okay. In attachment you can download a Logo server for testing and additional files to see the Modbus addresses of different operands. Maybe this will help you. Regards, Scorp AttachmentModbusServer.zip (176 Downloads) |
8/14/2020 9:55 PM | |
Posts: 10 Rating: (0) |
Hello. Sorry guys but too busy working over the week so not much time for the problem and reply. Scorp, all its installed and working properly in my opinion (check the attachment), before i wasn't sure even if on Easyio shows the connected client 1. I try to create more links from Logo to Easyio and shows more strait away, also when i disconnect logo connected devices go to 0 in easyio when i connect back shows again. Looks like they do communicate but don't send the data. Also in my opinion to configure Logo its enouth to use the network imput and should work. I think the best way will be to contact Easyio support, they must now Logo. Scorp EasyIo are fantastic compacted small controllers for simple automation like HVAC plants or lighting control but too slow for factory processes. Have a look at this https://www.syxthsense.com/controllers/easyio-sedona-controllers/ Thanks you both, for help. Regards. AttachmentEasyIo kits.zip (166 Downloads) |
Follow us on