8/27/2020 1:20 PM | |
Joined: 1/23/2013 Last visit: 8/10/2022 Posts: 226 Rating:
|
Hello test adapter USB LON Honeywell IF-LON ? Desigo LON AttachmentIF-LON.pdf (293 Downloads) |
8/27/2020 6:00 PM | |
Joined: 11/8/2017 Last visit: 7/24/2024 Posts: 328 Rating:
|
Hi, I haven't seen the Honeywell device before, so can't comment on it. From the datasheet that you attached, I see it is a TP/FT-10 device, which is correct for Desigo PX/RX. In general, the recommendation is to use the Gesytec Easylon USB Interface + LVU. See HERE for more info on the Gesytec device. PDF attached as well. Regards, AttachmentEasylon-Desigo_App_Note-EN-v1.0.pdf (268 Downloads) |
Follow us on