9/6/2020 6:13 PM | |
Posts: 1 Rating:
|
Good afternoon, Please i am having a communication problem between Simotion D435 - 2 and the field device of station No 2 (servo motor with encoder). These two error messages; 1: F0073 Drive control system - no ready signal 2: F0405 Station 2 station drive failure. are permanently displayed on on the HMI causing the machine no to run. Kindly assist Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/07/2020 10:58:25New subject after splitting |
|
9/7/2020 6:19 AM | |
Joined: 5/12/2006 Last visit: 9/3/2024 Posts: 22352 Rating:
|
and which device is it exactly? |
Follow us on