9/16/2020 8:41 AM | |
Posts: 17 Rating:
|
Okay, I bought a licence to pass from the version 15.1 to the version 16 of the firmware. I will try it when I will get it. Thank you |
9/16/2020 8:26 PM | |
Joined: 7/7/2010 Last visit: 7/3/2024 Posts: 14899 Rating:
|
Firmware 4.4 (which also means Portal V16 I think) is required for LHTTP_POST and related library components to compile. Are you using s7-1200 that can be updated to Firmware 4.4 and portal V16 is acceptable? I assume you need to use DNS resolution for the SAP server (in case I.T. moves it to another device with a different IP address). Attached is 1.0.1ß and I really do mean ßeta. It should compile on firmware less than 4.4. If it works, I'll be amazed at how well Siemens structured the original FB to make that even possible with simple gutting techniques. This will not handle FQDN that includes https at all. It is not good for anyone except you for your specific use case. Even then, it is not provided with any guarantee of performance or even functionality. As noted in Siemens TCP_QDN documentation, it needs that trailing "." to be considered fully qualified.
AttachmentLHTTP_Post_v1.0.1b.zip (333 Downloads) |
Last edited by: 0_Einstein at: 09/16/2020 20:27:47Last edited by: 0_Einstein at: 09/16/2020 21:13:44science guy |
|
This contribution was helpful to
1 thankful Users |
Follow us on