10/12/2020 7:46 AM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating: (2169)
|
Hello Mr.Joseph, you need to upgrade at least to WinCC V7.3 SE. The project can you migrate with the installed WinCC V7.3 SE. see: https://support.industry.siemens.com/cs/ww/en/view/97493192 5. Ordering data
Georg Berghof |
PS: If this post did really help you, you may use the Rate-button |
|
10/13/2020 4:31 AM | |
Joined: 2/12/2020 Last visit: 10/14/2024 Posts: 22 Rating: (0) |
Hello bg2492, Can I upgrade to WinCC 7.4 version? Thanks and Best Regards! |
10/13/2020 6:38 AM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating: (2169)
|
Hello Mr.Joseph, yes, you can upgrade to WinCC V7.4 or V7.5. Both versions are released for using on Microsoft Windows Server 2012 R2 Standard Edition (64-Bit) see compatibility tool https://support.industry.siemens.com/kompatool/pages/main/index.jsf?sitc=wwdfi10002 But only for V7.4 you can get a license upgrade from V7.x to V7.4. For V7.5, you need to upgrade the license to V7.2 at first, Regards Georg Berghof |
PS: If this post did really help you, you may use the Rate-button |
|
Follow us on