11/3/2020 9:12 AM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating: (2145)
|
Hello xmnj, you need to install in any case the DVD "Simatic_WinCCV7.5_SP1". The WinCC V7.5 SP1 without any Updates has known communication https://support.industry.siemens.com/cs/de/en/view/109773812
Georg Berghof |
PS: If this post did really help you, you may use the Rate-button |
|
This contribution was helpful to2 thankful Users |
11/6/2020 8:22 AM | |
Joined: 9/30/2016 Last visit: 4/5/2024 Posts: 910 Rating: (6) |
Please also see the attached screenshots. So which packages should I include to maintain the same functionality in 7.5 as I have in 7.4? AttachmentWCC75.zip (63 Downloads) |
11/6/2020 1:24 PM | |
Joined: 9/30/2016 Last visit: 4/5/2024 Posts: 910 Rating: (6) |
Please also see the attached screenshots. Would the "default settings" as shown in the screenshots be OK or do I need to make adjustments and if so which adjustments? AttachmentEPC upgrade.zip (54 Downloads) |
Follow us on