11/30/2020 12:10 PM | |
Posts: 9 Rating:
|
Still stuck with this one. Any help would be greatly appreciated :) |
12/4/2020 10:36 AM | |
Posts: 9 Rating:
|
S7 1200 |
12/4/2020 11:46 AM | |
Joined: 3/30/2020 Last visit: 9/4/2024 Posts: 4720 Rating:
|
We are a bit in the dark with what your application look like. The volume data and where that data is flowing to, is for example important. One method is to use (socket) Ethernet TCP or UDP. You may want to look at the following 3rd party project: |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
12/4/2020 12:02 PM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating:
|
hi Tom, Have a look into the communication settings of your CPU: Cycle load due to communication Try to set the maximum cycle load for communication ot the maximum of 50%. It also depends on the network and how you access the PLC. regards, |
FCK WAR! |
|
12/4/2020 1:21 PM | |
Joined: 10/18/2006 Last visit: 7/9/2024 Posts: 120 Rating:
|
Hi Tom_1122, if you are look for a ready and easy to use solution, look here: Or may be Node-RED can also be an option? |
iba AG - Data Acquisition and Analysis the way it should be |
|
Follow us on