12/7/2020 6:08 AM | |
Joined: 10/22/2011 Last visit: 7/31/2024 Posts: 299 Rating: (1) |
yes I know it is not easy. Thanks for link, this is what I want. |
12/9/2020 8:59 AM | |
Joined: 10/22/2011 Last visit: 7/31/2024 Posts: 299 Rating: (1) |
hello I have checked online diagnostics. Alarm are attached. please check and tell me the solution Thanks |
12/9/2020 9:01 AM | |
Joined: 5/12/2006 Last visit: 8/14/2024 Posts: 22343 Rating: (3003)
|
that only the simotion alarms you need also the sinamics faults |
12/9/2020 9:05 AM | |
Joined: 10/22/2011 Last visit: 7/31/2024 Posts: 299 Rating: (1) |
diagnostic buffer is attached AttachmentDevice Diagnostics11.txt (212 Downloads) |
12/9/2020 9:10 AM | |
Joined: 10/22/2011 Last visit: 7/31/2024 Posts: 299 Rating: (1) |
please check attachment |
12/9/2020 9:23 AM | |
Joined: 5/12/2006 Last visit: 8/14/2024 Posts: 22343 Rating: (3003)
|
300021 isd ground fault |
12/9/2020 9:38 AM | |
Joined: 10/22/2011 Last visit: 7/31/2024 Posts: 299 Rating: (1) |
but if we install old DMM, then motor is running fine without any problem and trip. so what could be the reason? |
Follow us on