12/15/2020 7:24 PM | |
Posts: 1 Rating: (0) |
i have a question which is simular, but couldnt get the answer from this post. I have been using a logo since 10 years but now have the oba8 and try to use the app to swith an output. Everyting is workig finr but i need to enter a box to change the value"edit set tag value" what could be the allowable value for switching a Network Input with adres V3.1? wheni try to change this via the Variables menu it works fine, i can just enter 1 or 0 and theinput changes in the Logo, but cant get the button to work. Thanks Pieter ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/16/2020 10:40:16New subject after splitting |
|
Follow us on