1/22/2009 12:03 AM | |
Posts: 2661 Rating: (279)
|
Check the following FAQ: Why are there values struck through in the SIMATIC WinCC V5.x Tag Logging Table Control? |
1/22/2009 11:52 AM | |
Joined: 8/27/2008 Last visit: 4/25/2024 Posts: 54 Rating: (1) |
Dear Phantom75, The archiving cycles and the acquisition cycleare exacly the same regards, rami |
1/22/2009 8:12 PM | |
Posts: 2661 Rating: (279)
|
Hi, Which version (+SP+HF) of WinCC are you using? I tried with WinCC V6.2 SP2 and it works fine. Regards |
1/29/2009 6:35 AM | |
Joined: 8/27/2008 Last visit: 4/25/2024 Posts: 54 Rating: (1) |
Dear Phantom75, I am using V6.2 SP2 (V6.2.2.0) as well. Regards, rami |
Follow us on