(0)| 2/4/2009 11:02 AM | |
|
Posts: 5 Rating:
|
Hi, Am running a program on a LOGO 24 transistor type module that is controlling a test rig for several hundred thousand cycles. I've written a program that is running ok but wanted to know if there were any better ways of controlling the timer function - the last timer seems a little off to the rest of them due to the reset signal I've generated from the last output. The program is to run four cylinders for 0.75 seconds each, with the same duration between the next cylinder coming on. Would appreciate any suggestions or improvements - am learning every day with this, and thats not such a bad thing! Plus I've got a few more test rigs to write similar programs for and it would help to use better practices from the start! Thanks Attachmenthoriz fatig.pdf (1384 Downloads) |
Follow us on