3/8/2021 3:29 PM | |
Joined: 9/27/2006 Last visit: 5/2/2024 Posts: 12257 Rating: (2666) |
Hello reypapin; There are different WinCC applications each with different versions. For example, this is the section of the WinCC v7.5 SP1 communications that shows different OPC interfaces. https://support.industry.siemens.com/cs/ww/en/view/109773067/125515441163 Note that OPC comes in various "flavors", OPC DA, HDA, more recently UA... So, which version of WinCC do you want to implement an OOC client on, and which flavour of OPC does your CD600 suport? Hope this helps, Daniel Chartier |
Follow us on