3/10/2021 1:33 PM | |
Joined: 2/10/2015 Last visit: 4/30/2024 Posts: 30 Rating: (2) |
Hi, I sent this post for share the solution, résolved with Siemens support very nice job thanks again So, the 1st one: -Edit your "Hosts" folder (target: Windows-->System32-->drivers-->etc) must be opened with the notepad in Admin mode Give to the two hosts (client/server) this is information : -Ip address from local machine and the network name -Ip address from destination/host Save Then make sure the Server OPC as the same login Finally follow this procedure, don't forget when you edit DCOM parameters --> Restart your machine https://support.industry.siemens.com/cs/fr/en/view/109483815 I hope that it will serve you See you |
Last edited by: The Helping Hand at: 03/11/2021 10:53:28Optimized link |
|
This contribution was helpful to1 thankful Users |
Follow us on