3/13/2021 3:12 PM | |
Joined: 9/27/2006 Last visit: 6/20/2024 Posts: 12260 Rating: (2671) |
Hello Regian; You can connect the Sitrans FVA 250 to a HART network, if you insert a MEM transducer HART 4-20mA (there are 2 models, one with additional pulse output). Both give you access to a totaliser value, it seems. https://support.industry.siemens.com/cs/ww/en/view/67676175 See the screenshot below. But you have to build up your PC to a HART modem in order to read the HART variables, and you "might" need PDM software to configure the PVA250 to your specs. You should talk to a Siemens instrumentation tech to ensure you work with this flowmeter correctly. Hope this helps, |
Follow us on