3/12/2021 12:25 PM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1054)
|
hi AP-TECH, Modbus RTU is a Protocoll designed for RS485. I don´t think that it works with converter like this. there are special Modbus converter that converts between different Modbus protocolls. S7-PLCs are able to communicate over Modbus TCP over the internal Ethernet interfaces. To make them communicating to Modbus RTU devices, you need a converter from Modbus TCP to Modbus RTU or a CP that provides a Modbus RTU interface, like CM1241: How do you establish a MODBUS-RTU communication with STEP 7 (TIA Portal) for the SIMATIC S7-1200?I recommend you to use the HW from this FAQ. hope this helps, regards, |
FCK WAR! |
|
This contribution was helpful to1 thankful Users |
Follow us on