6/5/2023 6:10 PM | |
Joined: 11/24/2022 Last visit: 6/7/2023 Posts: 1 Rating: (0) |
Good day every one i have to use both of soft starter model 3RW4047-1TB04 to operate 2 pumps with 45 KW each the problem happen as an ground fault when just power on the system (not even start pumps), the ground limit is 3.5 Mohm and I know it is may be accepted but i need to know why this happen? the ground fault disappear and problem solved when i take out lead A1 and A2 while the 3 phase power is applied on soft starter. so, what is the relation between A1 and A2 and ground, knowing the this ground fault appear in 2 system with total 4 soft starters and 4 pumps.. please help! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 06/06/2023 07:58:41New subject after splitting |
|