11/21/2006 8:14 AM | |
Posts: 3149 Rating: (171)
|
Hi, which WinCC / microsoft version are you using? Could you please post your WinCC diagnose files in the forum? nemo |
11/21/2006 10:24 AM | |
Posts: 66 Rating: (1) |
Hia and Thanks for the reply Nemo. Simatic WinCC K6.0.3.0, hotfix 2 (01010017) Where do I find the diagnose files? |
11/21/2006 12:23 PM | |
Posts: 3149 Rating: (171)
|
Hi, you will find the diagnose files in the folder ...\wincc\diagnose Are you using a lot of scripts? Then the APDIAG-tool can give usefull hints for programming errors http://support.automation.siemens.com/WW/view/en/22196555 nemo |
11/22/2006 1:11 PM | |
Posts: 66 Rating: (1) |
Hia! Really appreciate your help Nemo! I'm using internal tags for the status tags. Included are zip file from c:\programfiles\Siemens\WinCC\Diagnose Is this the files you need? Please let me know if you need anything else! Thanks V AttachmentWinCC_Op_01.zip (294 Downloads) |
Last edited by: vidarv at: 11/22/2006 1:36 PM |
|
11/22/2006 2:40 PM | |
Posts: 3149 Rating: (171)
|
Hi, your diagnosefiles just show some minor entries ...where/how do you set this status-tag? By scripting or by tags from your S7-CPU? nemo |
11/24/2006 6:19 PM | |
Posts: 66 Rating: (1) |
Hia All! Any ideas out there? I struggeling and can't find the reason, and stat up on the plant is on Monday! Best regards Vidar |
12/4/2006 9:53 AM | |
Joined: 9/27/2005 Last visit: 11/27/2007 Posts: 1398 Rating: (150)
|
Hi SP4 can be ordered from this link. It is a simple upgrade but you will need to upgrade any optional packages you are using (see this linkfor details). The recommended method of developing a running system is to use an Engineering Station (ES) - much the same as PCS7 does. Changes should be made on the ES and then downloaded to the server while it is still running. This way you do not need to restart runtime on the server nor mess around with log files. If you have a separate spare machine then I would recommend you implement an ES as this should make life a lot easier. It does require an extra WinCC licence for the ES machine but this is a small price to pay for a working, recommended system. Salma |
Follow us on