5/1/2016 8:51 AM | |
Posts: 84 Rating: (19) |
Hi, Do anyone can help me to get a html code to display alarm page similar like we have in HMI. |
5/1/2016 6:51 PM | |
Posts: 198 Rating: (36) |
HI Creating and using user-defined web pages on S7-1200 in this above link sample of user defined web page study in program tank level overflow this is a kind of alarm you can see in program and web page to how its work I think this is answer of your question. In addition to the standard mechanisms of the web page such as identification, diagnostic buffer, module status, communication, variable status and data log, individual web pages can be designed and called for your particular application. This application shows how to create your own user-defined web pages for S7-1200 easily and quickly. Prior knowledge in HTML-programming is not absolutely necessary. To create your individual web page (user-defined web page), you can use any tools such as Microsoft FrontPage, Notepad, etc.. For designing your web page, you can use all options provided by HTML, CSS and JavaScript. In addition, there is a special command syntax (AW P command) for directed communication with the CPU. The following figure shows the implemented visualization:
|
5/1/2016 11:48 PM | |
Posts: 198 Rating: (36) |
Creating and using user-defined web pages on S7-1200 / S7-1500 read page 28 of attach pdf or select above page article below Simple examples for the webserver of SIMATIC S7-1200 / S7-1500 (2,2 MB) Attachmentalarm page28_Simple_Web_Examples_DOCU_v10_en (3).pdf (400 Downloads) |
2/22/2018 4:47 PM | |
Joined: 4/25/2015 Last visit: 4/30/2024 Posts: 96 Rating: (4) |
Is this solved? Is it with S7-1500? |