8/21/2019 8:52 AM | |
Joined: 12/10/2014 Last visit: 5/9/2024 Posts: 6 Rating: (0) |
Hello all, I need to alarm the derivative datapoint as soon as the high limit is exceeded. The alarm is coming but is generated at long intervals (see "Alert_list_View_Timestamps.png") also „Alert_list_by_email.png“. Perhaps it is related to the fact that the excess is recorded with a delay? The last 3 records are above the limit, but the system does not mark them as an alarm (see "Delayed_Alarming.png"). There are settings in other attached files. Please check the settings and any advice. AttachmentAtachement.zip (302 Downloads) |