2/18/2006 3:44 PM | |
Posts: 102 Rating: (3) |
Hai All See I have configured somewhere around 7 projects where I have Taken drives on profibus and every where all I have done is set the 10th bit of CW1 as 1 and use load tansfer statements for data transmission and its working. No. of drives on a single proffibus master system was 26. For the example you can see my briefcase at yahooUser name is shamsher.ppam@yahoo.com.The name of the project is s7proj1. Here I have used 7 drives on proffibus which send the status word both 1 and 2, actual speed, current and recieve the controll words and setpoint. Regards Shamsher |
6/14/2011 5:56 PM | |
Posts: 16 Rating: (0) |
Hi Shamsher, Could you send me some examples of drives integration projects to lord_t2ng@yahoo.com .Thank you |
6/14/2011 6:19 PM | |
Joined: 3/21/2006 Last visit: 7/26/2024 Posts: 10228 Rating: (1181)
|
SINAMICS / MICROMASTER 4: Use of STARTER and STEP7 V11 together with Siemens frequency converters Basically when you have Drive ES installed on the same PC with Step7 when you create a project there is available to insert a drive. And that's it. After using a routing (in most of the case) is possible to upload and download a parameters to a drive. Perhaps might be useful: http://support.automation.siemens.com/WW/view/en/23548709 best regards, Hristo Mihalev |
Follow us on