5/9/2012 11:49 AM | |
Joined: 8/27/2006 Last visit: 9/2/2024 Posts: 719 Rating: (88) |
In that case, I would Reinstall Windows |
The more you know, The more you know that you don't know |
|
5/9/2012 11:50 AM | |
Joined: 4/24/2006 Last visit: 9/12/2024 Posts: 8736 Rating: (1167) |
Hello algudkar, Perhaps this link might help: how do you clear message 256:26 "An OLE error has occurred"? Best regards, Wizard |
5/9/2012 12:35 PM | |
Posts: 621 Rating: (10) |
Hi wizard thank you for the rply i will try it! regards algudkar |
5/9/2012 6:25 PM | |
Posts: 557 Rating: (64) |
Hello, we can use online tool for checking purpose. see the link. https://support.automation.siemens.com/kompatool/pages/main/interim.jsf |
5/10/2012 7:19 AM | |
Posts: 621 Rating: (10) |
Hi wizard / friends icome back with you once again. exactly what you above mentioned OLE error 256:26. as per you given the link i was go through that and tryed to clear the error also.but same thing is there and un installed the software and again same version V5.4 SP5 software installed.nothing changed here i attached 2 photo snaps. the 2 snap is the same project i copied in the external disk.and trying to open the project.but now that popup which is in 2nd snap if i closed or click on ok the complete simatic manager window automatically closed. my friends are suggesting me that formate the PC and re installed the software.but i cont do this.because this is main server pc.in the customer site friends can you help me.... regards algudkar Attachmentscreens.zip (101 Downloads) |
Follow us on