12/2/2020 3:48 PM | |
Joined: 2/10/2015 Last visit: 8/21/2024 Posts: 288 Rating:
|
Is it possible to download a project edited under SIMOTION SCOUT with STARTER from a SINAMICS inverter. |
12/2/2020 4:09 PM | |
Joined: 5/12/2006 Last visit: 9/3/2024 Posts: 22352 Rating:
|
download (to inverter) or Upload (from inverter) ? |
12/2/2020 4:13 PM | |
Joined: 2/10/2015 Last visit: 8/21/2024 Posts: 288 Rating:
|
in both directions, i.e. upload from and download to |
12/2/2020 4:21 PM | |
Joined: 5/12/2006 Last visit: 9/3/2024 Posts: 22352 Rating:
|
upload from yes download to yes if you first perform upload from |
12/2/2020 6:33 PM | |
Joined: 2/10/2015 Last visit: 8/21/2024 Posts: 288 Rating:
|
In access point, I chose S7ONLINE and in PG / PC parameter, I chose my ethernet network card But, when I start the search for subscribers, I see the first message (add IP address / subnet masks) and I clicked on yes. Some time later, I perceive the second message telling me no device was found. I have STARTER V5.4.0.1 HF1 that I have installed and I don't know if the version of SINAMICS D425, CU320, S120 they used may not exist in my version of STARTER. When I installed SIMOTION SCOUT I managed to open the SIMOTION SCOUT source project from the simatic manager and I went online without problem. But, I uninstalled simotion to install starter because there is a machine with sinamic inverters programmed with starter. as I cannot have simotion and starter on my pc at the same time then, I decided to have starter alone and work with on the different machines. since i uninstalled simotion when i open my main project with simatic manager i have this software missing error message yet i have starter on the pc. see attached file.
AttachmentFILES.zip (214 Downloads) |
Follow us on