7/5/2014 11:44 AM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating: (2147) |
Hello Webpower, a simple way is to use an indirect adressing. This means, you use a string-tag in which you write the Tagname, which should be used. The other way is to use the function "SetLink" to change the connected tag to an object-property. See description for "SetLink" on page 1330 of "WinCC V7.2 Scripting: VBS, ANSI-C, VBA" http://support.automation.siemens.com/WW/view/en/73453640 Regards Georg Berghof |
PS: If this post did really help you, you may use the Rate-button |
|