4/13/2011 1:21 PM | |
Posts: 154 Rating:
|
Hello, following you can find a description to delete the password from the S7-200 manual. If you forget the password, you must clear the memory of the S7-200 and reload your program.Clearing the memory puts the S7-200 in STOP mode and resets the S7-200 to the factory-setdefaults, except for the network address, baud rate, and the time-of-day clock. To clear yourprogram in the S7-200:1. Select the PLC > Clear menu command to display the Clear dialog box. 2. Select all three blocks and confirm your action by clicking OK.3. If a password had been configured, STEP 7--Micro/WIN displays a password-authorizationdialog box. To clear the password, enter CLEARPLC in the password-authorization dialogbox to continue the Clear All operation. (The CLEARPLC password is not case sensitive.)The Clear All operation does not remove the program from a memory cartridge. Since the memorycartridge stores the password along with the program, you must also reprogram the memory With the wipeout.exe you can reset your PLC to the factory settings. Please also look here: link |
This contribution was helpful to
1 thankful Users |
10/4/2021 10:09 AM | |
Joined: 12/18/2014 Last visit: 9/15/2025 Posts: 35961 Rating:
|
Or take a look at this FAQ: Password for the access to a password-protected S7-200 does not exist |
10/4/2021 10:14 AM | |
Joined: 12/18/2014 Last visit: 9/15/2025 Posts: 35961 Rating:
|
Here's no help for password cracking ... |
10/4/2021 10:20 AM | |
Joined: 10/4/2021 Last visit: 8/16/2024 Posts: 3 Rating:
|
thanks maybe I lose my job |
Follow us on