5/11/2012 9:33 PM | |
Joined: 1/5/2007 Last visit: 4/7/2023 Posts: 1690 Rating: (580)
|
Hello,
In this case you find circuits for the LOGO!-series 0BA5 to 0BA7 which use the specific possibilities in each case. Special features are on the one hand in particular the utilization of the best time resolution of the LOGO! function blocks' with 0,01 s and on the other handthe extension of the possibilities... I hope, for everyone something is in this case (and at the attachnent)...
AttachmentDEMO_en_timer_stopwatch_and_more.zip (576 Downloads) |
==> Meine TAG-Listen: "deut." |
|
This contribution was helpful to5 thankful Users |