2/23/2016 7:07 PM | |
Joined: 4/28/2015 Last visit: 2/7/2024 Posts: 10533 Rating: (819) |
RECV instr. |
With best regards... |
|
2/23/2016 7:40 PM | |
Posts: 3093 Rating: (323)
|
Hello Duris, I checked the manual Simatic Net Program blocks it states (unfortunately only for S7-400 CPs) Case 2b: Sequence with TCP connections On a TCP connection, the length specified in the ANY pointer of the RECV parameter is the deciding factor. An FC6 /FC60 job is completed with the condition code NDR=1, as soon as an amount of data corresponding to the specified length has been written to the receive buffer. Regards, |
This contribution was helpful to2 thankful Users |
Follow us on