1/15/2014 7:22 PM | |
Posts: 5 Rating: (0) |
i have the same problem but with s7 1200. I have wincc 7.2 , i have connected the plc and the pc via the ethernet port but wincc can't communicate with plc. i have attached pictures. what i do wrong?
Attachmentwincc7.2.pdf (1393 Downloads) |
1/16/2014 8:55 AM | |
Posts: 5 Rating: (0) |
1. No i haven't change the name of access point.As i know, s7 protocol suite isn't suitable for s7 1200, for this reason i have chosen simatic s7-1200, s7-1500 channel. I tried with s7 protocol suite but it didn't work again. i saw in link below http://www.youtube.com/watch?v=92ylAUJ6ghQ and i did the same but nothing. i attached a photo with my all access point. 2. yes, Broadcom is a wireless interface. PlC is connected in a router. But i have tried to connect plc and my laptop with ethernet cable (Intel Gigabit interface in set pc/pg interface) but it didn't work.
Attachmentaccess point.pdf (890 Downloads) |
1/16/2014 4:20 PM | |
Posts: 510 Rating: (117) |
Loukas, When the Access Point in the connection shown in the Configuration Studio is associated with a valid network connection in the the PG/PC Interface and you can PING the PLC from the WinCC computer, you should be connected. See the attachment. Goog Luck, billwest
AttachmentWinCC_1500_Connection.pdf (1591 Downloads) |
9/18/2014 5:27 AM | |
Joined: 10/29/2007 Last visit: 5/24/2024 Posts: 59 Rating: (1) |
HiAlfredo@as99 I have same problem like you. There is no one"TCP / IP" protocolbut only"OMS+" inThe "SIMATIC S7-1200, S7-1500 Channel" channel. Did you slove your problem? Could you tell me how to slove this problem? An other question is: Can i use IE General port instead CP 1612,CP1613, CP1512as recomments from siemens? CP1612 was discontinuation, so can I use CP1612A2 instead CP1612?
|
6/21/2017 12:44 AM | |
Posts: 510 Rating: (117) |
I have attached a Step by Step for getting your S7-1500 connected to your WinCC V7.4, I hope this helps you. Good Luck! billwest AttachmentWinCC74_1500.pdf (741 Downloads) |
This contribution was helpful to2 thankful Users |