7/23/2020 12:36 PM | |
Joined: 12/26/2016 Last visit: 9/8/2021 Posts: 2 Rating: (0) |
Hello! Try to read this topic https://support.industry.siemens.com/tf/ww/en/posts/wincc-and-two-network-cards/151704/?page=0&pageSize=10 ! Solution is in the last message! I faced with the same trouble and the solutiond helped me! It is amazing, but in Set PC/PG tool both my adapters are active simultaneously. Also in WinCC in TCP/IP connection only one board can be selected. But they both are working, when runtime is launched! |