7/10/2020 11:27 PM | |
Joined: 6/20/2020 Last visit: 4/4/2024 Posts: 42 Rating: (0) |
Thanks ixo65,your answer helped me a lot, but i'm having the opposite problem now. The simulation works well but not the reality. in reality, the 1 / 10s counter increments to 32767 in a very short time. Here is my program in attached file. Pressing I3 starts the two counters. The counter 1s totals in liters. (never reset) The 1 / 10s counter totals the 5 sec cycle. It is reset on the next cycle. Thank you for your help.
AttachmentVolume Cycle-Total.zip (125 Downloads) |