9/2/2018 1:30 PM | |
Joined: 4/15/2018 Last visit: 5/12/2022 Posts: 5 Rating: (0) |
Why should we drop the voltage ? If the range of sensing the input as high should be between 18Vdc<V<24vdc (high bit).else if the voltage across the input terminal is less than 18vdc therefore , the plc considers it as low value(zero bit). So if you drop the voltage from 24 TO 5vdc the input wont count it as high but low .Any suggestions? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 9/3/2018 1:09:54 PMNew subject after splitting |
|