1/9/2012 10:08 PM | |
Joined: 3/11/2007 Last visit: 7/18/2024 Posts: 226 Rating: (13) |
Un esempio di invio email
AttachmentTest E-mail.zip (1595 Downloads) |
This contribution was helpful to6 thankful Users |
1/18/2012 10:00 PM | |
Posts: 1 Rating: (0) |
Where do I find the TM_Mail Block? |
1/18/2012 11:56 PM | |
Joined: 3/11/2007 Last visit: 7/18/2024 Posts: 226 Rating: (13) |
Hello, you must have version 11 and SP 2. |
11/5/2012 2:27 PM | |
Posts: 51 Rating: (1) |
Hello everyone, I am trying to send an email with test program from automatizzando (with my mail settings). I have a big problem with this, because when I try to send an email, I do not get any error STATUS from the TM_mail block and email is not sent from the PLC. What am I doing wrong? Best regards |
11/5/2012 2:48 PM | |
Joined: 7/7/2010 Last visit: 10/14/2024 Posts: 15302 Rating: (2427)
|
Maybe you could copy and then paste your settings, and replace the email addresses with xxxxx@xxxx.com and ip addresses with xxx.xxx.xxx.xxx and if it is a syntax issue, we can help with that. If it is like automatizzando's original issue with a gateway definition, we cannot tell you the solution to that kind of problem. If you have a portable usb drive and use a portable snmp email server for a temporary test, you could email from your plc to your pc's fake snmp mail server and see if it is actually a plc problem or a snmp email routing issue. I use portableapps.com but there are plenty of freeware portable apps that install on a thumb drive and help solve all kinds of problems. These little solutions run from the usb drive and do not require installation into the windows computer. |
science guy |
|
6/14/2013 1:48 PM | |
Joined: 6/8/2011 Last visit: 9/16/2022 Posts: 40 Rating: (25) |
Can You give me info how YOu make calculation of ip server addres to hex? In my case a have some problems. Best regards. 192.168.1.1 in hex 12539AB thats is correct? |
6/14/2013 2:59 PM | |
Joined: 4/21/2007 Last visit: 1/10/2024 Posts: 39 Rating: (0) |
The attached picture shows how I do the conversion right in my program. |
Follow us on